JAJSVV8 December 2024 AFE5401-EP
PRODUCTION DATA
Each channel has an associated 12-bit header register. These registers can be written by an SPI write. The content of this register can be read out on the CMOS data output (D[11:0]) by configuring the HEADER_MODE register, as shown in Table 7-18.
| HEADER_MODE | DESCRIPTION |
|---|---|
| 0 | ADC data at output |
| 1 | Header data at output |
| 2 | [Temperature data, diagnostic data, mean, noise, (-1), (-1), (-1), (-1)]. This data sequence is repeated. |
| 3 | Header data, temperature data, diagnostic data, mean, noise, ADC data |
In HEADER_MODE = 3, the header mode data output is shown in Figure 7-14.
In this mode, header data is transmitted with a latency with respect to the TRIG input. This latency is given by Equation 2:
Figure 7-14 Header Mode Data Output (HEADER_MODE = 3)