JAJSVV9 December 2024
PRODUCTION DATA
Figure 7-5 shows the input structure for the logic level pins INHx, INLx. INHx and non-inverted INLx has passive pull down, so when inputs are floating the output the gate driver will be pulled low. Figure 7-6 shows the input structure for the inverted INLx pins. The inverted INLx has passive pull up, so when inputs are floating the output of the low-side gate driver will be pulled low.
Figure 7-5 INHx and non-inverted INLx
Logic-Level Input Pin Structure
Figure 7-6 Inverted INLx Logic-Level Input Pin
Structure