JAJU657 December 2018
The MSP430FR2633 operates in Active mode while the user is touching any sensor on the CAPT-BSWP board. The measured current averages approximately 480 µA in this mode.
When the sensors are no longer being touched, the CPU enters low power mode LPM3 indefinitely and the CapTIvate peripheral is configured to operate in wake-on-proximity mode. In this mode, the CapTIvate peripheral is only looking for the presence of a finger or hand, waking the CPU if detected. Operating in this wake-on-proximity mode, the CPU can achieve very low power. The measured current averages approximately 5 µA in this mode.
Two methods are available to measure the MSP430FR2633 power consumption.
For either option, return jumper J3 to the original position when done.
NOTE
The MSP430F5529 LaunchPad development kit must be disconnected from the MSP430FR2633 MCU board during the measurement. The MSP430FR2633 MCU board continues to respond normally to finger gestures.
For more information about current measurements on the MSP430FR2633, refer to the Experiments with Low Power section of the CapTIvate™ Technology Guide.
| Test Conditions (Method 1) | Result |
|---|---|
| Active mode | 480 µA |
| Low power, Wake on Proximity | 5 µA |