SBAU279 October 2020
Alerts can be enabled and configured on the Alert Configuration tab as shown in Figure 3-9. Channels configured as digital outputs (CH7) in Section (Channel Selection) can be enabled as the Alert output channel. In Figure 3-9 the Alert is mapped to CH-7 and will trigger based on the threshold levels for CH0 (AIN0) that were configured in Section (Input Channel Configuration).
Figure 3-9 Channel Configuration tab - Alert Configuration.