SBAU353 October   2021

 

  1.   Trademarks
  2. 1EVM Overview
    1. 1.1 ADS131A04EVM Kit
    2. 1.2 ADS131A04EVM Board
  3. 2ADS131A04EVM Quick Start Guide
  4. 3EVM Analog Interface
    1. 3.1 ADC Analog Input Signal Path
    2. 3.2 ADC External Clock (XTAL1/CLKIN and XTAL2) Options
  5. 4Digital Interface
    1. 4.1 SPI Communication
    2. 4.2 Connection to the PHI
    3. 4.3 Digital Header
    4. 4.4 LaunchPad Connectors
  6. 5Power Supplies
  7. 6ADS131A04EVM Initial Setup
    1. 6.1 Default Jumper Settings
    2. 6.2 EVM Graphical User Interface (GUI) Software Installation
  8. 7ADS131A04EVM Software Reference
    1. 7.1 EVM GUI Global Settings for ADC Control
    2. 7.2 Register Map Configuration Tool
    3. 7.3 Time Domain Display Tool
    4. 7.4 Spectral Analysis Tool
    5. 7.5 Histogram Tool
  9. 8ADS131A04EVM Bill of Materials, PCB Layout, and Schematic
    1. 8.1 Bill of Materials
    2. 8.2 PCB Layout
    3. 8.3 Schematic
  10. 9References

ADS131A04EVM Quick Start Guide

The following instructions are a step-by-step guide to connecting the ADS131A04EVM to the computer and evaluating the performance of the ADS131A04:

  1. Review the default jumper settings in Section 6 and GUI software installation in Section 6.2.
  2. Connect the ADS131A04EVM to the PHI. Install the two screws as indicated in Figure 2-1.
  3. Use the provided USB cable to connect the PHI to the computer.
    1. LED D5 on the PHI lights up, indicating that the PHI is powered up
    2. LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC. Figure 2-1 shows the resulting LED indicators.
      GUID-20210924-SS0I-KCXJ-NMGJ-RH5HWPXQJNHZ-low.jpg Figure 2-1 ADS131A04EVM Hardware Setup and LED Indicators
  4. Launch the ADS131A04EVM GUI software as by clicking the ADS131A04EVM executable shown in Figure 2-2.
    GUID-6264358E-3BB8-435B-BC49-C6A40B481671-low.gif Figure 2-2 Launch the EVM GUI Software
  5. Click the Wake Up and then Unlock button in the Single commands section of the GUI and start using the ADS1282EVM GUI to evaluate the EVM as shown in Figure 2-3. Learn more about EVM GUI Global Input Parameters and the various pages within the GUI in Section 7.1.
    GUID-0A082358-3A0D-4CA8-A444-7912E6B45FE6-low.gif Figure 2-3 EVM GUI Global Input Parameters