SBAU417A July 2025 – September 2025
Run Script file: Run a script file by first selecting the file in the Scripts window and then by pressing F5 (or selecting Run and then Buffer in the menu bar).
Run part of script: Run part of a script file by selecting the lines in the Editor window and then by pressing F7 (or selecting Run and then Run Selection in the menu bar).
Stop Execution: Stop the current execution by pressing F10 (or selecting Run and then Stop in the menu bar).
Clear Session: The current session can be cleared to reset the Latte UI to its initial state by pressing Ctrl-T (or selecting Session and then Clear Session in the menu bar). This process is equivalent to a restart and can be used to restart a session without closing the GUI.