SBAU487 August 2025
Using the provided USB to serial cable, plug the USB end into the PC and connect the 9-pin D connector into the RS-232 port on the EVM. Apply 3.3V to J5 and run the calibrator executable file. LEDs D1 and D2 illuminate and the following screen appears on the PC.
If the COMMS button does not turn green, verify there is +3.3V applied to J5 and double-check the COM port settings in both the Device Manager and calibrator-config.XML file. Press the COMMS button to launch the metering GUI. The screen in Figure 3-4 showing the meter status becomes active on the computer.