SBAU489 June 2025
Figure 2-3 shows a diagram identifying three filters. Use these three circuit filters to adjust the AMC-MOD-50A-EVM performance. With each filter, there is a tradeoff between noise and propagation delay. The weaker the filter, the shorter the propagation delay.
The following equation calculates the cutoff frequency for the input filter.
Selecting a shunt resistor with high inductance when measuring a high frequency signal potentially causes overshoot in AC measurements. Overshoot caused by parasitic inductance is compensated for with proper design of the differential RC filter. Best input filter design is dependent on the inductance of the resistor and PCB design. Figure 3-6 shows an example simulation for TINA-TI.
The following equation calculates the cutoff frequency for the DOUT and CLKIN filters. Modify as needed for bandwidth limitations.