SBOA523 July   2021 TMP390 , TMP392

 

  1.   Trademarks
  2. 1Temperature Switch Introduction
    1. 1.1 Temperature Switch Design Using Discrete Components
    2. 1.2 Replacing Discrete Solutions With TMP390
  3. 2Alternative Applications
  4. 3Conclusion
  5. 4References

Temperature Switch Introduction

The ability to detect and react to thermal events within a system is not only a paramount aspect of safety, but also a strong factor in being able to optimize system performance. There are many applications in which thermal management is important, including DC/AC inverters, DC/DC converters, temperature transmitters, environmental control systems (ECS), power tools, power banks, and wireless infrastructure. The simplest solution is to create a temperature switch that toggles based on certain thresholds that the user sets, and will alert the user should the temperature exceed the set thresholds. Figure 1-1 shows an example of the desired operation of a temperature switch.

GUID-D20FB26F-332E-4AF3-AF71-7F4DEDA21C40-low.gifFigure 1-1 Temperature Switch Output With Hot or Cold Thresholds and Hysteresis

There are two outputs that both have active low logic. Each output corresponds to a channel and each channel corresponds to a threshold. In this example, Channel A corresponds to the hot threshold while channel B corresponds to the cold threshold, both of which can be specified by the user. In addition, there is an option of hysteresis of either 5°C or 10°C. This behavior is recreated with the three subsequent designs presented in this report.