SBOA582 November   2023 OPA2387 , OPA387 , OPA4387 , RES11A , RES11A-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction to Differential Signaling
  5. 2Common-Mode Rejection Ratio in Difference Amplifier Circuits
  6. 3Improving CMRR with Precision Matched Resistor Divider Pairs, RES11A-Q1
  7. 4Derive Differential and Common-Mode Gain, Difference Amplifier
  8. 5Derive CMRR for Discrete Resistor Tolerance
  9. 6Derive CMRR for Matched Ratio Tolerance
  10. 7Summary
  11. 8References

Derive CMRR for Discrete Resistor Tolerance

A common assumption in difference amplifier circuits is that the ratio of R4 and R3 is equal to the ratio of R2 and R1, as described by Equation 23.

Equation 23. R 4 R 3 = R 2 R 1   =   R g R i n

This assumption is useful because it allows the differential gain equation to be reduced to the form in Equation 24. This is the simplified gain equation for a difference amplifier circuit.

Equation 24. A D = R g R i n

Combining Equation 23 with Equation 20 shows that if the resistor ratios are perfectly matched, the common-mode gain (ACM) is 0 V/V, and therefore the common-mode rejection ratio of the resistor network (CMRRR) is infinite.

Equation 25. A C M = R g R i n + R g - R g R i n + R g R i n R i n + R g =   0   V / V

In practice, the variation in absolute resistance due to resistor tolerance produces mismatches between the absolute ratios of R4/R3 and R2/R1. The ratio mismatch presents an asymmetrical resistor divider effect at the amplifier's input terminals. Any common-mode input voltage is attenuated unequally between the two resistor dividers and presents as a small differential voltage which is amplified by the differential gain of the circuit, thus degrading the CMRR performance of the differential stage.

Considering a differential amplifier circuit consisting of four discrete resistors with tolerance t, the worst-case ratio matching occurs when the absolute resistor values differ from the nominal resistor values as shown in Figure 5-1 in which,

Equation 26. R 1 = R 1 N 1 + t
Equation 27. R 2 = R 2 N 1 - t
Equation 28. R 3 = R 3 N 1 - t
Equation 29. R 4 = R 4 N 1 + t

Where,

  • RXN is the nominal resistance of resistor RX in Ω
  • t is the absolute tolerance of the resistor in Ω/Ω
GUID-20231012-SS0I-LKPD-JWND-KTQHB5BDKZ6L-low.svg Figure 5-1 Worst-Case Resistor Matching of Difference Amplifier Circuit

The nominal resistor ratios determine the nominal gain of the difference amplifier stage.

Equation 30. R 4 N R 3 N = R 2 N R 1 N = G

Where,

  • RXN is the nominal resistance of resistor RX in Ω
  • G is the nominal differential gain of the amplifier stage in V/V

The contribution of resistor tolerance to the overall common-mode rejection ratio of the difference amplifier can be determined in the worst-case by combining Equation 26 through Equation 29 with Equation 22.

Equation 31. C M R R R = 1 2 2 R 2 N R 4 N ( 1 - t ) ( 1 + t ) + R 1 N R 4 N ( 1 + t ) 2 + R 2 N R 3 N ( 1 - t ) 2 R 1 N R 4 N ( 1 + t ) 2 - R 2 N R 3 N ( 1 - t ) 2

Applying the relationship defined in Equation 30,

Equation 32. C M R R R = 1 2 2 G 2 R 1 N R 3 N ( 1 - t 2 ) + G R 1 N R 3 N ( 1 + t ) 2 + G R 1 N R 3 N ( 1 - t ) 2 G R 1 N R 3 N ( 1 + t ) 2 - G R 1 N R 3 N ( 1 - t ) 2

Which reduces to

Equation 33. C M R R R = G + 1 + t 2 ( 1 - G ) 4 t

Standard resistor tolerances are very small, typically 1% or less, therefore it is common to further simplify the equation for t << 1. The contribution of discrete resistor tolerance to the overall CMRR of the difference amplifier for t << 1 is defined by Equation 34.

Equation 34. C M R R R G + 1 4 t

Where,

  • G is the nominal differential gain in V/V
  • t is the absolute tolerance of the resistors in Ω/Ω