SCDA036 May 2022 TMUX8212
Because Photorelays and Multiplexers are solid state devices with no moving parts, they do not have the issue of bouncing like mechanical relays. Bouncing occurs when a mechanical relay changes state. Because the switch is physical, there is a period where the switch bounces between the on and off state before settling. Additionally, Photorelay and Multiplexers can be hot switched (turned on/off when a voltage is present on the switch) with no impact to reliability for the same reason. In a mechanical relay, this hot switching can wear down or even weld the contactors causing severe issues with reliability.
Another key benefit of multiplexers is their much faster turn on/off time. Mechanical Relays turn on/off in the order of 1-10ms. Photorelays improve on this to about 0.1-1ms. Multiplexers improve even more to about 50-500us. This can increase operation speed and remove potential synchronization errors in the system. Another important performance difference is that Photorelay turn on/off time is dependent on the LED drive current. As the forward current on the LED increases, the turn off time increases. Multiplexers have no such dependency and switch at a constant speed regardless of the GPIO drive voltage.