SFFS361 March 2022 TPSM82864A , TPSM82866A
This section provides a failure mode analysis (FMA) for the pins of the TPSM8286xA. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 2-2 through Table 2-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 2-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
Figure 2-1 shows the TPSM8286xA pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPSM8286xA data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
EN |
1 |
The device will not be enabled. |
B |
PG |
2 |
Loss of PG functionality |
B |
VSET/MODE |
3 |
Intended functionality for the adjustable output voltage configuration in power save mode. For the fixed output voltage configuration, the output voltage will be regulated to 0.6 V. |
B |
PGND |
4, 5, 6, 8, 9, 10, 11, 19, 20 |
Intended functionality |
D |
SW |
7 |
Potential device damage |
A |
VOUT |
12, 13, 14, 15 |
No output voltage |
B |
VOS |
16 |
No output voltage |
B |
FB |
17 |
Output voltage will not be regulated. The device will enter 100% mode. |
B |
AGND |
18 |
Intended functionality |
D |
VIN |
21, 22 |
The device is not functional. |
A |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
EN |
1 |
Undetermined state of the pin. The device may or may not be enabled. |
B |
PG |
2 |
Loss of PG functionality |
B |
VSET/MODE |
3 |
Will operate in forced PWM mode. If configured for the fixed output voltage configuration, the output voltage will be regulated to 0.6 V. |
B |
PGND |
4, 5, 6, 8, 9, 10, 11, 19, 20 |
Redundant pin. If one of the pins are open, there is no functionality loss but there is a potential impact on device performance. |
C |
SW |
7 |
Intended functionality |
D |
VOUT |
12, 13, 14, 15 |
Redundant pin. If one of the pins are open, there is no functionality loss but there is a potential impact on device performance. |
C |
VOS |
16 |
Output voltage regulation will be worse. |
C |
FB |
17 |
The device is not functional. Open loop operation |
B |
AGND |
18 |
The device is not functional. |
B |
VIN |
21, 22 |
Redundant pin. If one of the pins are open, there is no functionality loss but there is a potential impact on device performance. |
C |
Pin Name | Pin No. | Shorted to | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|---|
EN |
1 |
PG |
2 |
Loss of EN and PG functionality. Potential device damage |
A |
PG |
2 |
VSET/MODE |
3 |
Intended functionality for the adjustable output voltage configuration in power save mode. For the fixed output voltage configuration, the output voltage will be regulated to 0.6 V. If configured for forced PWM mode operation, there is potential device damage. |
A |
VSET/MODE |
3 |
PGND |
4 |
Intended functionality for the adjustable output voltage configuration in power save mode. For the fixed output voltage configuration, the output voltage will be regulated to 0.6 V. If configured for forced PWM mode operation, the device is not functional. |
A |
PGND |
6 |
SW |
7 |
Potential device damage |
A |
PGND |
11 |
VOUT |
12 |
No output voltage |
B |
VOUT |
15 |
VOS |
16 |
Intended functionality |
D |
VOS |
16 |
FB |
17 |
Intended functionality for the fixed output voltage configuration. For the adjustable output voltage configuration, the output voltage will be regulated to 0.6 V. |
B |
FB |
17 |
AGND |
18 |
Output voltage will not be regulated. The device will enter 100% mode. |
B |
AGND |
18 |
PGND |
19 |
Intended functionality |
D |
PGND |
20 |
VIN |
21 |
The device is not functional. |
A |
VIN |
22 |
EN |
1 |
Loss of EN functionality |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
EN |
1 |
Loss of EN functionality |
B |
PG |
2 |
Loss of PG functionality. Potential device damage |
A |
VSET/MODE |
3 |
Intended functionality for the adjustable output voltage configuration in forced PWM mode. For the fixed output voltage configuration, the output voltage will be regulated to 0.6 V. |
B |
PGND |
4, 5, 6, 8, 9, 10, 11, 19, 20 |
The device is not functional. |
A |
SW |
7 |
Potential device damage |
A |
VOUT |
12, 13, 14, 15 |
Potential device damage |
A |
VOS |
16 |
Potential device damage |
A |
FB |
17 |
Output voltage will not be regulated. If configured in forced PWM mode, there is potential device damage. |
A |
AGND |
18 |
The device is not functional. |
A |
VIN |
21, 22 |
Intended functionality |
D |