SFFS663 september 2023 LMQ644A2-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the LMQ644xx-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1, Figure 4-2, and Figure 4-3 show the LMQ644xx-Q1 pin diagrams. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LMQ644xx-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN2 | 1 | VOUT = 0 V | B |
CB2 | 2 | VOUT = 0 V | B |
SW2 | 3 | Potential Damage to HS FET | A |
PGND3 | 4 | Normal Operation | D |
SW1 | 5 | Potential Damage to HS FET | A |
CB1 | 6 | VOUT = 0 V | B |
VIN1 | 7 | VOUT = 0 V | B |
SERIES_CAP1 | 8 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND1 | 9 | Normal Operation | D |
SYNC | 10 | Normal operation for PFM mode. | C |
PG1 | 11 | Loss of Power Good Flag | B |
MODE | 11 | Normal operation for PFM mode. | C |
EN1 | 12 | Device is Disabled | C |
BIAS/VOSNS1 | 13 | VOUT1 = 0V short circuit | B |
FB1 | 14 | If configured as 3.3V fixed, normal operation. If configured for other Vout, then Vout1 will be out of specification and output 3.3V | B |
VCC | 15 | Device is Disabled | B |
AGND | 16 | Normal Operation | D |
RT | 17 | VOUT = 0 V. No switching. | B |
FB2 | 18 | If configured as 3.3V fixed, normal operation. If configured for other Vout, then Vout2 will be out of specification and output 3.3V | B |
SS | 18 | VOUT = 0 V | B |
VOSNS2 | 19 | VOUT2 = 0V if FB2=VCC or GND. | B/C |
COMP | 19 | VOUT = 0 V | B |
EN2 | 20 | Second Channel is disabled | B |
CONFIG | 21 | Device is Configured as Dual Output Voltage | B |
PG2 | 22 | Loss of Power Good Flag | B |
SYNCOUT | 22 | If primary, secondary and tertiary devices will not switch. If secondary, tertiary device will not switch. If tertiary, no effect | B |
PGND2 | 23 | Normal Operation | D |
SERIES_CAP2 | 24 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND | 25 | Normal Operation | D |
Pin Name | Pin No | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN2 | 1 | VOUT2 = 0V | B |
CB2 | 2 | VOUT2 will collapse under load as FET gate voltage is not enough to fully enhance. Damage may occur if current is pulled from switch. | A |
SW2 | 3 | VOUT2 = 0V | B |
PGND3 | 4 | Normal Operation | D |
SW1 | 5 | VOUT1 = 0V | B |
CB1 | 6 | VOUT1 will collapse under load as FET gate voltage is not enough to fully enhance. Damage may occur if current is pulled from switch. | A |
VIN1 | 7 | VOUT1 = 0V | B |
SERIES_CAP1 | 8 | Normal Operation | D |
PGND1 | 9 | Normal Operation | D |
SYNC | 10 | Device can toggle between PFM and PWM modes | C |
PG1 | 11 | Loss of Power Good Flag | B |
MODE | 11 | Device can toggle between PFM and PWM modes | C |
EN1 | 12 | Loss of Disable Function | C |
BIAS/VOSNS1 | 13 | If in fixed output configuration, Vout >> than set point. If in adjustable Vout configuration, slight increase in input current. | B |
FB1 | 14 | Part configuration will be randomly selected between Fixed 5V or Adjustable. | B/C |
VCC | 15 | Part can turn on and off as VCC uvlo is triggered. | B |
AGND | 16 | Normal Operation | D |
RT | 17 | VOUT = 0 V. No switching. | B |
FB2 | 18 | Part configuration will be randomly selected between Fixed 5V or Adjustable. | B/C |
SS | 18 | Fast Soft Start | D |
VOSNS2 | 19 | If in fixed output configuration, Vout >> than set point. | B |
COMP | 19 | Device can have oscillations on VOUT | B |
EN2 | 20 | Loss of Disable Function | C |
CONFIG | 21 | VOUT = 0 V. No switching. | B |
PG2 | 22 | Loss of Power Good Flag | B |
SYNCOUT | 22 | If primary, secondary and tertiary devices will not switch. If secondary, tertiary device will not switch. If tertiary, no effect | B |
PGND2 | 23 | Normal Operation | D |
SERIES_CAP2 | 24 | Normal Operation | D |
PGND | 25 | Normal Operation | D |
Pin Name | Pin No | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN2 | 1 | Boot driver will be damaged | A |
CB2 | 2 | VOUT2 = 0 | B |
SW2 | 3 | Potential Damage to HS FET | A |
PGND3 | 4 | Potential Damage to HS FET | A |
SW1 | 5 | VOUT1 = 0 | B |
CB1 | 6 | Boot driver will be damaged | A |
VIN1 | 7 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
SERIES_CAP1 | 8 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND1 | 9 | Normal operation for AUTO mode. | C |
SYNC | 10 | For PG < 5.5V. Device will start in PFM and transition to PWM after start up. For PG > 5.5V damage may occur. For mode, part might enter PFWM of PWM mode based on SYNC logic | A |
PG1 | 11 | For EN < 20V. Device damage could occur if PG FET current limit is exceed. For EN > 20V, PGOOD FET can be damaged. | A |
MODE | 11 | For EN < 20V. Normal Operation For EN > 20V, PGOOD FET can be damaged. | A |
EN1 | 12 | For EN < 5V. Output voltage out of range. For EN > 5V, device damge can occur if current is not limited | A |
BIAS/VOSNS1 | 13 | If configured as 3.3V fixed, normal operation. If configured for other Vout, then Vout1 will be out of specification and output 3.3V | B |
FB1 | 14 | If configured as 5V fixed, normal operation. If configured for other Vout, then Vout1 will be out of specification and output 5V | B |
VCC | 15 | Vout1 = Vout 2 = 0V | B |
AGND | 16 | VOUT = 0 V. No switching. | B |
RT | 17 | Switching Frequency and output voltage will be incorrect. | B |
FB2 | 18 | If FB2 is grounded, Vout2 >> than set point. If FB2 is VCC then VCC will be pulled to 5V, no damage should occur. If FB2 is resistor divider the Vout will be 3.3Vout and see a load from the FB resistance to ground. | B |
SS | 18 | Fast Soft Start | C |
VOSNS2 | 19 | VOUT2 >> than set point | B |
COMP | 19 | EN > 5.5V. Damage of comparator if not current limited. | A |
EN2 | 20 | EN2 < 5.5V. Device is Configured as Dual Output Voltage. EN2 > 5.5 damge if not current limited | A |
CONFIG | 21 | Device is Configured as Dual Output Voltage | B |
PG2 | 22 | Loss of Power Good Flag | B |
SYNCOUT | 22 | If primary, secondary and tertiary devices will not switch. If secondary, tertiary device will not switch. If tertiary, no effect | B |
PGND2 | 23 | Normal Operation | D |
SERIES_CAP2 | 24 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND | 25 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
Pin Name | Pin No | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN2 | 1 | Normal Operation | D |
CB2 | 2 | Boot driver will be damaged | A |
SW2 | 3 | Potential Damage to LS FET | A |
PGND3 | 4 | VOUT = 0 V | B |
SW1 | 5 | Potential Damage to LS FET | A |
CB1 | 6 | Boot driver will be damaged | A |
VIN1 | 7 | Normal Operation | D |
SERIES_CAP1 | 8 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND1 | 9 | VOUT = 0 V | B |
SYNC | 10 | Potential Damage for VIN > 5.5V | A |
PG1 | 11 | Loss of Power Good Flag. Potential Damage if not current limited | A |
MODE | 11 | Normal operation for PWM mode. Potential Damage for VIN > 5.5V | A |
EN1 | 12 | Device is enabled | C |
BIAS/VOSNS1 | 13 | Potential damage from permanent short across converter | A |
FB1 | 14 | Potential Damage for VIN > 5.5V | A |
VCC | 15 | Potential Damage for VIN > 5.5V | A |
AGND | 16 | VOUT = 0 V | B |
RT | 17 | Potential Damage for VIN > 5.5V | A |
FB2 | 18 | Potential Damage for VIN > 5.5V | A |
SS | 18 | Potential Damage for VIN > 5.5V | A |
VOSNS2 | 19 | Potential Damage for VIN > 5.5V | A |
COMP | 19 | Potential Damage for VIN > 5.5V | A |
EN2 | 20 | Second Channel is enabled | C |
CONFIG | 21 | Potential Damage for VIN > 5.5V | A |
PG2 | 22 | Potential Damage for VIN > 20V or lower if not current limited | A |
SYNCOUT | 22 | Potential Damage for VIN > 5.5V or lower if not current limited | A |
PGND2 | 23 | VOUT = 0 V | B |
SERIES_CAP2 | 24 | Series Capacitor is shorted internally. Device bypassing capacitance will increase as two series capacitors becomes single capacitor. | D |
PGND | 25 | VOUT = 0 V | B |