SFFSAZ4 November   2025 LMP8640-Q1

 

  1.   1
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
  6. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the LMP8640-Q1 and LMP8640HV-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the LMP8640-Q1 and LMP8640HV-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LMP8640-Q1 and LMP8640HV-Q1 data sheets.

LMP8640-Q1 LMP8640HV-Q1 Pin
                                        Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • TA = –40°C to +125°C
  • V+ = 12V; V- = 0V
  • V+IN = V-IN = 42V
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VOUT1Output is pulled down to GND and output current is short-circuit limited. When left in this configuration for a long time, under high supplies, self-heating can cause the die junction temperature to exceed 150°C.B
V-2The device operates as normal.D
+IN3In a high-side configuration, a short from the bus supply to GND occurs.B
-IN4In a high-side configuration, a short from the bus supply to GND occurs (through RSHUNT). High current flows from the bus supply to GND. The shunt can be damaged. In a low-side configuration, The device operates as normal.B for high-side
D for low-side
NC5The device operates as normal.D
V+6Power supply shorted to GND.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VOUT1Output can be left open. There is no effect on the device, but the output is not measured.C
V-2No power to the device. The device can be biased through inputs. Output is no longer referenced to GND.B
+IN3The shunt resistor is not connected to the amplifier. The IN+ pin can float to an unknown value. Output goes to an unknown value, not to exceed Vs or GND.B
-IN4The shunt resistor is not connected to the amplifier. The IN- pin can float to an unknown value. Output goes to an unknown value, not to exceed Vs or GND.B
NC5The device operates as normal.D
V+6No power to device. Device can be biased through inputs. Output is incorrect and close to GND.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
VOUT12 – V-Output is pulled down to GND and output current is short-circuit limited. When left in this configuration for a long time, under high supplies, self-heating can cause the die junction temperature to exceed 150°C.B
V-23 – +INPower supply is shorted to GND.B
+IN34 – -INInputs are shorted together, so no sense voltage is applied. Output stays close to REF potential.B
-IN45 – NCThe device operates as normal.D
NC56 – V+The device operates as normal.D
V+61 – VOUTOutput is pulled to Vs and the output current is short-circuit limited. When left in this configuration for a long time, under high supplies, self-heating can cause the die junction temperature to exceed 150°C.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to Vs
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VOUT1Output is pulled to Vs and the output current is short-circuit limited. When left in this configuration for a long time, under high supplies, self-heating can cause the die junction temperature to exceed 150°C.B
V-2Power supply is shorted to GND.B
+IN3In a high-side configuration, the device power supply is shorted to the bus supply (through RSHUNT). In a low-side configuration, the device power supply is shorted to GND.B
-IN4In a high-side configuration, the device power supply is shorted to the bus supply. In a low-side configuration, the device power supply is shorted to GND (through RSHUNT).B
NC5The device operates as normal.D
V+6The device operates as normal.D