SFFSAZ5 December 2025 INA790A , INA790B , INA791A
Figure 4-1 shows the INA79X-Q1 pin diagrams for the DEK (VQFN – 15) package. For a detailed description of the device pins please refer to the corresponding Pin Configuration and Functions sections in the INA790x and INA791x datasheets.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN+ | 1 | A short from the bus supply to GND occurs. High current flows from the bus supply to GND. Damage to the internal bond wires is possible. | A |
| NC | 2 | The device operates as normal. | D |
| VS | 3 | The power supply is shorted to GND. There is no power to the device. | B |
| NC | 4 | The device operates as normal. | D |
| GND | 5 | The device operates as normal. | D |
| NC | 6 | The device operates as normal. | D |
| NC | 7 | The device operates as normal. | D |
| IS– | 8 | In a high-side configuration, a short from the bus supply to GND occurs. High current flows from the bus supply to GND. The shunt is potentially damaged due to high current. | A |
| In a low-side configuration, normal operation. | D | ||
| IN– | 9 | In a high-side configuration, a short from the bus supply to GND occurs. High current flows from the bus supply to GND. Damage to the internal bond wires is possible. | A |
| In a low-side configuration, normal operation. | D | ||
| NC | 10 | The device operates as normal. | D |
| OUT | 11 | The output is shorted to GND. | B |
| FB | 12 | The output voltage becomes unpredictable. | B |
| REF | 13 | The device operates as normal if REF = GND by design. | D |
| If REF ≠ GND by design, the functionality of the device is affected. | B | ||
| ALERT | 14 | The ALERT pin is forced to active mode. There is a loss of the functionality of the ALERT pin. | B |
| IS+ | 15 | A short from the bus supply to GND occurs in a high-side configuration. The functionality of the system is affected in a high-side or low-side configuration. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN+ | 1 | The device operates as normal. | D |
| NC | 2 | The device operates as normal. | D |
| VS | 3 | There is no power to the device. | B |
| NC | 4 | The device operates as normal. | D |
| GND | 5 | There is no power to the device. | B |
| NC | 6 | The device operates as normal. | D |
| NC | 7 | The device operates as normal. | D |
| IS– | 8 | The bus supply to the load path is cut off and load current does not flow. | C |
| IN– | 9 | The device operates as normal. | D |
| NC | 10 | The device operates as normal. | D |
| OUT | 11 | The output can be left open. | C |
| FB | 12 | The output becomes unpredictable | B |
| REF | 13 | The output becomes unpredictable | B |
| ALERT | 14 | The ALERT pin is open. There is a loss of the functionality of the ALERT pin. | B |
| IS+ | 15 | The bus supply to the load path is cut off and load current does not flow. | C |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| IN+ | 1 | 2 – NC | The device operates as normal. | D |
| NC | 2 | 3 – VS | The device operates as normal. | D |
| VS | 3 | 4 – NC | The device operates as normal. | D |
| NC | 4 | 5 – GND | The device operates as normal. | D |
| GND | 5 | 6 – NC | The device operates as normal. | D |
| NC | 6 | 7 – NC | The device operates as normal. | D |
| NC | 7 | 8 – IS– | The device operates as normal. | D |
| IS– | 8 | 9 – IN– | The device operates as normal. | D |
| IN– | 9 | 10 – NC | The device operates as normal. | D |
| NC | 10 | 11 – OUT | The device operates as normal. | D |
| OUT | 11 | 12 – FB | The device operates as normal if the OUT pin is shorted to the FB pin by design | D |
| If the OUT pin is not shorted to the FB pin by design, the functionality of the device is affected. | C | |||
| FB | 12 | 13 – REF | The functionality of the output is affected. | C |
| REF | 13 | 14 – ALERT | The functionalities of both the output and ALERT pins are affected. | B |
| ALERT | 14 | 15 – IS+ | In a high-side configuration, damage to the device is possible. | A |
| In a low-side configuration, there is a loss of the functionality of the ALERT pin. | B | |||
| IS+ | 15 | 1 – IN+ | The device operates as normal. | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN+ | 1 | In a low-side configuration, a short from the pin VS to GND occurs. In a high-side configuration, the bus supply is shorted to the VS pin. Damage to the device is possible. | A |
| NC | 2 | The device operates as normal. | D |
| VS | 3 | The device operates as normal. | D |
| NC | 4 | The device operates as normal. | D |
| GND | 5 | The power supply is shorted to GND. There is no power to the device. | B |
| NC | 6 | There is a slight increase in quiescent current. The device functionality not affected. | C |
| NC | 7 | The device operates as normal. | D |
| IS– | 8 | In a high-side configuration, a short from the bus supply to the VS pin occurs. High current flows from the bus supply to the VS pin or from the VS pin to the bus supply. Damage to the device is possible. | A |
| In a low-side configuration, the functionality of the system is affected negatively but the device is not negatively affected. | C | ||
| IN– | 9 | In a high-side configuration, a short from the bus supply to the VS pin occurs. High current flows from the bus supply to the VS pin or from the VS pin to the bus supply. Damage to the device is possible. | A |
| In a low-side configuration, the functionality of the system is affected negatively but the device is not negatively affected. | C | ||
| NC | 10 | The device operates as normal. | D |
| OUT | 11 | The output is shorted to the power supply. | B |
| FB | 12 | The output becomes unpredictable. | B |
| REF | 13 | The device operates as normal if REF = VS by design. | D |
| If REF ≠ VS by design, the functionality of the device is affected. | B | ||
| ALERT | 14 | There is a loss of the functionality of the ALERT pin. | B |
| IS+ | 15 | In a low-side configuration, a short from the VS pin to GND occurs. In a high-side configuration, the bus supply is shorted to the VS pin. Damage to the device is possible. | A |