SLAAEK3 January 2024 MSPM0G3507
This subsystem demonstrates how to implement the MSPM0 device as a UART to SPI bridge. Incoming UART packets are expected to be in a specific format in order to facilitate SPI communication. This example also has the ability to determine error conditions and communicate them back to the UART device. The code for this example can be found in the MSPM0 SDK.