SLAU292G November 2009 – July 2015
For first time use, remove the eZ430-Chronos from box and press any button twice to wake the Chronos module from sleep mode. After the first button press, the LCD displays the same content as shown on the box of the kit, and after the second button press, the Chronos module starts full operation.
NOTE
For the next steps it is important to understand the eZ430-Chronos user concept. The top and bottom LCD lines can be controlled individually by pushing the buttons on the left side. The buttons on the right side are used to select or activate secondary functions. Detailed instructions are available in Section 3.2.