SLAU533D September 2013 – April 2017
Device Manager is very useful for determining what USB interfaces have enumerated on the host.
To open Device Manager, click the Start button, click Run…, type "devmgmt.msc" in the Open field, and click OK (see Figure 35).
If Windows asks if you want to allow the program to make changes to your computer, click Yes; however, Device Manager is very useful for viewing purposes without having to change anything (see Figure 36).
The groups in Device Manager that are relevant to MSP430 USB work include:
Device Manager is also very useful during debug of a USB application. The MSP430 USB API Programmer's Guide in the MSP430 USB Developers Package contains a section on how to debug your USB application. See this document for more information on using Device Manager.