SLAU748B October   2017  – September 2018 MSP432E401Y

 

  1.   SimpleLinkrep%#8482; Ethernet MSP432E401Y Microcontroller LaunchPad™ Development Kit (MSP-EXP432E401Y)
    1.     Trademarks
    2. 1 Board Overview
      1. 1.1 Kit Contents
      2. 1.2 Using the Ethernet LaunchPad Development Kit
      3. 1.3 Features
      4. 1.4 BoosterPack Plug-in Modules
      5. 1.5 Specifications
    3. 2 Hardware Description
      1. 2.1 Functional Description
        1. 2.1.1 Microcontroller
        2. 2.1.2 Ethernet Connectivity
          1. 2.1.2.1 RJ-45 Connections
        3. 2.1.3 USB Connectivity
        4. 2.1.4 Motion Control
        5. 2.1.5 User Switches and LEDs
        6. 2.1.6 BoosterPack Plug-in Modules and Headers
          1. 2.1.6.1 BoosterPack Plug-in Module Interface 1
          2. 2.1.6.2 BoosterPack Plug-in Module Interface 2
          3. 2.1.6.3 Breadboard Connection
          4. 2.1.6.4 Other Headers and Jumpers
        7. 2.1.7 Serial Bootloader
      2. 2.2 Power Management
        1. 2.2.1 Power Supplies
        2. 2.2.2 Low Power Modes
        3. 2.2.3 Clocking
        4. 2.2.4 Reset
      3. 2.3 Debug Interface
        1. 2.3.1 XDS-110 Debug Interface
        2. 2.3.2 External Debugger
        3. 2.3.3 Virtual COM Port
    4. 3 Software Development
      1. 3.1 Software Description
      2. 3.2 Source Code
      3. 3.3 Tool Options
      4. 3.4 Programming the Ethernet LaunchPad Development Kit
    5. 4 PCB Schematics
  2.   Revision History

Programming the Ethernet LaunchPad Development Kit

The SimpleLink MSP432E4 SDK includes projects for each of the example applications for the different supported tool chains. If you installed the SimpleLink MSP432E4 SDK to the default installation path of C:\ti\, you can find the example applications in C:\ti\ simplelink_msp432e4_sdk_<version>\examples\. The onboard XDS-110 is used with the supported toolchain to program applications on the MSP-EXP432E401Y LaunchPad development kit.

Follow these steps to program example applications into the Ethernet LaunchPad development kit using the XDS-110:

  1. Install a toolchain on a PC running Microsoft Windows.
  2. Connect the USB-A cable plug in to an available USB port on the PC and plug the Micro-B plug to the XDS-110 USB port at the top of the MSP-EXP432E401Y LaunchPad development kit.
  3. Verify the RED LED on the left side of the XDS-110 is illuminated.
  4. Run the toolchain and import the project. Build the project to generate the toolchain specific output file.
  5. Press on the download and debug button for the toolchain to download the code.
  6. After the code has been downloaded to the MSP-EXP432E401Y LaunchPad development kit, run the code.