SLLA486A May   2020  – May 2021 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044

 

  1.   Trademarks
  2. When Do I Need to Isolate CAN?
  3. What are the Options Available to Isolate CAN Bus?
  4. Now That I Have Isolated CAN Signal Path, How Do I Generate Isolated Power?
  5. What’s the Reason Behind Terminating the Bus, Do I Need it, and How to Achieve it?
  6. What’s the Difference Between Common Mode Range and Bus Standoff Mentioned in Data Sheet?
  7. Now That I Have Taken Care of the Termination Resistor, What Other Components do I Need on the Bus Side?
  8. When Connecting Isolated CAN Nodes in a Network, What Should be Done with the Floating Bus-Side Ground Connection?
  9. Is There a Limitation on Minimum Data Rate That I Can Operate? What About the Maximum Data Rate Achievable in a Network?
  10. Is There a Limit on Maximum Number of Nodes That I Can Connect in CAN Network?
  11. 10What Factors Decide the Maximum Communication Distance in a CAN Network?
  12. 11What is the Maximum Value of Bus Capacitance That Can be Introduced Between CANH to GND and CANL to GND? Can Higher Capacitance Damage the Device?
  13. 12Is There a Way to Extend the Maximum Communication Distance?
  14. 13What is Stub Length? What are the Design Considerations Around it?
  15. 14I am Seeing Larger Differential CAN Voltage for Some Bits of CAN Packet Compared to Rest of the Packet When I am Communicating in a Network with Multiple Nodes Connected. Why?
  16. 15References
  17. 16Revision History

When Connecting Isolated CAN Nodes in a Network, What Should be Done with the Floating Bus-Side Ground Connection?

Since CAN is a differential interface, the entire network will work fine if just two wires for CANH/CANL are interconnected between all nodes of a network, as long as common mode voltage of CAN lines with respect to bus-side ground of the receiving CAN node is within its recommended operating conditions. However, under noisy-system scenarios, best practice is to use a third ground reference line and connect it between all nodes. This way, receiver of each CAN node has a reference, and common mode voltage range will not be violated. If the cable is shielded, the shield can act as a common ground reference with shield connected to earth potential at just one node to avoid any ground loops. Proper system design can ensure large common mode voltages induced on the CAN bus (due to noise pickup) drop across the isolation barrier by connecting the logic-side ground of the isolated CAN transceiver to local ground.