SLLU091A January 2006 – September 2022
The basic setup in Figure 6-1 has the two power supplies required to evaluate isolator performance with 3.3-V on one side and 5-V on the other. If both sides are to be evaluated at the same supply voltage, only one power supply is required and can be used to power both sides of the EVM.
Note that this EVM is for operating parameter performance evaluation only and not designed for isolation voltage testing. Any voltage applied above the 5.5-V maximum recommended operating voltage of the ISO721 will damage the EVM.
Figure 6-1 Basic EVM OperationThe input to the EVM is a 20-MHz pulse displayed on channel 1 in Figure 6-2. The output of the EVM is channel 2.
Figure 6-2 Typical Input and Output Waveforms