SLUAA11B February 2020 – August 2021 BQ769142 , BQ76922 , BQ76942 , BQ76952
The RESET subcommand performs a reset on the device and returns RAM register settings back to default (or OTP programmed) values. This command is issued by writing 0x0012 to 0x3E.
| Command | Name | Description |
|---|---|---|
| 0x0012 | RESET | Resets the device. |
Figure 2-4 Captured I2C Waveform of RESET
SubcommandThe Transaction Log in this example shows all of the commands that have been covered for executing Subcommands.
Figure 2-5 BQStudio Example Showing
Execution of Multiple Subcommands