SLUAAO7 March   2023 BQ24640 , BQ25173 , BQ25713 , BQ25798

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Supercapacitors Charging Key Care-Abouts and Implementations
    1. 2.1 Supercap Charge Profile
    2. 2.2 Linear Based Supercap Charger
    3. 2.3 Switch-Mode Buck Converter Based Supercap Charger
    4. 2.4 Modifying Li-ion Chargers to Charge Supercaps
    5. 2.5 Using a Li-ion Buck-Boost Integrate FET Charger to Charge a Supercap or Li-ion Battery
    6. 2.6 Using a Buck-Boost Controller with External FETs to Charge a Supercap
  5. 3Summary
  6. 4References

Using a Buck-Boost Controller with External FETs to Charge a Supercap

Modifying an integrated FET, host controlled buck-buck boost charger to charge a supercap is best if

  • The input voltage to the charger can be higher or lower than VREG.
  • ICHG is high, typically > 3.0A
  • The supercap’s capacitance is very high or very fast charging time is required
Unlike many chargers, the BQ25713/30 family of buck-boost charge controllers with external FETs does not provide trickle charge. Also, even though it is an NVDC charger, the BQ25713/30 has I2C registers that allow the user to disable the minimum system voltage, and therefore precharge phase, and BAT pin short circuit protection. With the minimum system voltage disabled, the voltage across the BATFET during initial charge is minimized.

If a minimum system voltage is needed, the controller's minimum system voltage can be enabled and set to the lowest acceptable value for the system, to minimize losses across the BATFET.

The BQ25713 block diagram is shown below. The host sets the charge current and supercap voltage regulation, as well as the other settings previously mentioned, in the charger's I2C registers.

GUID-20230316-SS0I-BHLZ-SKSP-064P4PLF8VBP-low.svgFigure 2-9 BQ25713 Charger Block Diagram

A complete charge cycle using the BQ25713 to charge a 5 F supercap to 5.2 V with ICHG = 3 A from VBUS = 20 V is shown in Figure 2-10.

GUID-20230111-SS0I-BQXB-NXPS-2JKFFHBMJS0C-low.pngFigure 2-10 BQ25713 Charge Cycle of a 5 F Supercap with ICHG = 3 A

As shown in the curve in Figure 2-10, the charger requires a minimum output voltage (approximately 2 V) to supply a given charge current, so V(SYS) is maintained at this level until V(BAT) = V(CAP) rises up to V(SYS). Initially, there is high but slowly decreasing power loss (PL(MAX) = 2 V * ICHG) in the BATFET. The user must select a BATFET which can safely handle this power dissipation, especially if their charge current is high.