Before powering up the test procedure, make
sure that the connections are correct as shown as in Section 3.3.
- Turn on PSU #1 and check the current on
DMM #1. If the current shown is more than 0.5mA and less than 1.25mA, then everything is
set correctly.
- Turn on the function generator output and
examine for the following conditions:
- The current on DMM #1 with the
function generator ON must show 2.7mA±1mA.
- The OUT signal must have a narrower
width compared to the IN signal. Use Figure 4-2 as reference.
- Look at the FAULT signal, this must
be high at all times except when the OUT signal is low during the period where IN is
high. When IN becomes low, the FAULT rises to high again. Use Figure 4-2 as reference.
- There must be a 5V signal on
VREF.
- Once testing is satisfied, power down the
EVM by following the order:
- Turn off function generator.
- Turn off power supply #1.
- Disconnect cables and probes.
Note: To learn more about why the Out-The-Box Evaluation causes this
behavior to occur, see
Section 2.5.