SLUUCY9 November 2023
The EVM is constructed with a single connection to the top and bottom of the cell stack. Cell voltage for these cells is sensed on the board.
The cell simulator provides resistors between the cell inputs. When the cell simulator shunts are installed, these resistors load the cells and divide the voltage to any unconnected inputs as cells are connected. If desired, then the cell simulator shunts can be installed during cell connection and removed after cell connection. The shunts must be removed after connection of cells or the cells are discharged by the constant drain of the cell simulator resistors.
BAT- is the reference voltage for the IC and must be connected first. After BAT- cells can be connected in any order. Cell connection from the bottom up minimizes the voltage step size applied to the board. Recommended connection sequence for the EVM when connecting cells is bottom up:
Figure 3-5 shows an example connecting cells with an EVM configuration reduced to 4 cells.