SLUUCZ3A July 2024 – March 2025
Measure the voltages at the correct location to evaluate the efficiency of the power train (device and inductor). This action is necessary because otherwise the efficiency measurements include losses that are not related to the power train. Losses incurred by the voltage drop in the copper traces and input and output connectors are not related to the efficiency of the power train, which must not be included in efficiency measurements.
Input current is measured between the input supply and EVM input in the input wires, and output current is measured in the output wires between the EVM and load.
Table 4-1 shows the measurement points for input and output voltage. VIN and VOUT are measured to calculate the dc-dc converter efficiency. Using the VIN and VOUT measurement points results in efficiency measurements that excluded losses due to the wires and connectors.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| PVIN_SNS+ | PVIN_SNS | Input voltage measurement point for PVIN | The pair of test points are connected to the PVIN/PGND pins of U1. The voltage drop between input terminal to the device pins is included for efficiency measurement. |
| PVIN_SNS- | PGND_SNS | Input voltage measurement point for PGND | |
| VOUT_RMT | VOUT_RMT | Output voltage measurement point for VOUT | The pair of test points are connected near the output terminals. The voltage drop from the output point of the inductor to the output terminals is included for efficiency measurement. |
| GND_RMT | GND_RMT | Output voltage measurement point for PGND |
For more accurate efficiency measurements of the power train, remove the voltage drop between the power train and the terminals from the measurement. Using the test points in Table 4-2 reduces these losses.
| Test Point | Node Name | Description | Comment |
|---|---|---|---|
| PVIN_SNS+ | PVIN_SNS | Input voltage measurement point for PVIN | The pair of test points are connected to the PVIN/PGND pins of U1. The voltage drop between input terminal to the device pins is included for efficiency measurement. |
| PVIN_SNS- | PGND_SNS | Input voltage measurement point for PGND | |
| VOUT_EFF | VOUT_EFF | Output voltage measurement point for VOUT | This pair of test points are connected to VOUT and GND near the output inductor for U1 and U1 PGND. |
| GND_EFF | GND_EFF | Output voltage measurement point for PGND |