SLUUDD5 September   2025

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Quick Start Guide
  6. 3Home Screen
  7. 4Starting a New Simulation
  8. 5Running the Simulations and Outputs

Running the Simulations and Outputs

Once a design has been created or imported, the user can now simulate the design by selecting the red “Simulate” button at the bottom of the 2D slice window, as shown in Figure 5-1.

 Simulation Button Figure 5-1 Simulation Button

Once the user initiates the simulation, the 2D slice window displays an animation of the light source moving in an arc above the sensor. The light source sweeps from -90 degrees to +90 degrees, and the amount of light illuminating the sensor area for each angle of incidence is logged in the background. Once the simulation is complete, the angular response graph is displayed to the right side of the simulation window, as shown in Figure 5-2.

 Angular Response Plot Figure 5-2 Angular Response Plot

On the top right of the plot window, the user can expand the plot as shown in Figure 5-3 and Figure 5-4.

 Expand Icon Figure 5-3 Expand Icon
 Expanded Angular Response
                    Graph Figure 5-4 Expanded Angular Response Graph

The generated plot is interactive, meaning you can hover over the different angles and view the sensor response, as shown in Figure 5-5.

 Plot Hover Feature Figure 5-5 Plot Hover Feature

For multi-channel sensors like the OPT4048 (XYZ sensor) and the OPT4003 (ALS + IR sensor), the plot contains the angular response for all channels. Figure 5-6 and Figure 5-7 depicts the angular response of a 4-channel and 2-channel sensor, respectively.

 4-Channel Color Sensor Angular
                    Response Figure 5-6 4-Channel Color Sensor Angular Response
 2-Channel Sensor Angular
                    Response Figure 5-7 2-Channel Sensor Angular Response

For further analysis, users can export the different plot points in excel format by selecting the “export” button on the top left of the plot window (see Figure 5-8).

 Export Button Figure 5-8 Export Button