SLVAEU4A June   2020  – November 2025 TPS61175-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS61175-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality.
B No device damage, but loss of functionality.
C No device damage, but performance degradation.
D No device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS61175-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS61175-Q1 datasheet.

TPS61175-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is used within the Recommended Operating Conditions and the Absolute Maximum Ratings sections found in the TPS61175-Q1 datasheet.
  • The configuration is as shown in the Application and Implementation section found in the TPS61175-Q1 datasheet.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SW 1 The power supply is short. There is potential damage to the inductor and pin. A
2 The power supply is short. There is potential damage to the inductor and pin. A
VIN 3 The power supply is short. The device does not operate. B
EN 4 There is a loss of the ENABLE function. The device remains in shut-down mode. B
SS 5 The device does not operate. B
SYNC 6 The output voltage is correct. There is a loss of the SYNC function. C
AGND 7 There is no effect on the device. D
COMP 8 The device does not operate. B
FB 9 The output voltage is extremely high. The device is potentially damaged. A
FREQ 10 The switching frequency is extremely high. The device is potentially damaged. A
NC 11 There is no effect on the device. D
PGND 12 There is no effect on the device. D
13 There is no effect on the device. D
14 There is no effect on the device. D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SW 1 The device is potentially damaged. A
2 The device is potentially damaged. A
VIN 3 There is a loss of power supply. The device does not operate. B
EN 4 There is a loss of the ENABLE function. The device remains in shut-down mode. B
SS 5 There is a loss of the soft start function. C
SYNC 6 The device is easily coupled by noise. B
AGND 7 The internal signals have no reference ground. The device is potentially damaged. A
COMP 8 The output voltage cannot regulate. The device is potentially damaged. A
FB 9 The output voltage cannot regulate. The device is potentially damaged. A
FREQ 10 The device does not operate. B
NC 11 The device is potentially damaged. A
PGND 12 When one of the repetitive pins is left open, there is no effect to the function of the pin. D
13 When one of the repetitive pins is left open, there is no effect to the function of the pin. D
14 When one of the repetitive pins is left open, there is no effect to the function of the pin. D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
SW 1 SW There is no effect on the device. D
SW 2 VIN The device is potentially damaged. A
VIN 3 EN The output voltage is correct. There is a loss of the ENABLE function. C
EN 4 SS The SS pin is damaged if the voltage of the EN pin is higher than 7V. A
SS 5 SYNC The device does not operate. B
SYNC 6 AGND The output voltage is correct. There is a loss of the SYNC function. C
COMP 8 FB The output voltage cannot regulate. The device is potentially damaged. A
FB 9 FREQ The output voltage cannot regulate. The device is potentially damaged. A
FREQ 10 NC The switching frequency is extremely high. The output voltage is incorrect. B
NC 11 PGND There is no effect on the device. D
PGND 12 PGND There is no effect on the device. D
PGND 13 PGND There is no effect on the device. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SW 1 The device is potentially damaged. A
2 The device is potentially damaged. A
VIN 3 There is no effect on the device. D
EN 4 The output voltage is correct. There is a loss of the ENABLE function. D
SS 5 The SS pin is damaged if the supply voltage is higher than 7V. A
SYNC 6 The SYNC pin is damaged if the supply voltage is higher than 7V. A
AGND 7 There is high current out of the power supply. The device does not operate. B
COMP 8 The COMP pin is damaged if the supply voltage is higher than 3V. A
FB 9 The FB pin is damaged if the supply voltage is higher than 3V. A
FREQ 10 The FREQ pin is damaged if the supply voltage is higher than 3V. A
NC 11 The device is potentially damaged. A
PGND 12 There is high current out of the power supply. The device does not operate. B
13 There is high current out of the power supply. The device does not operate. B
14 There is high current out of the power supply. The device does not operate. B