SLVAFE4 june   2023 TLC6983

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Common issues in NPP Matrix LED Panel
    1. 2.1 Ghosting
    2. 2.2 Non-Uniformity in Low Gray Scale
    3. 2.3 Coupling
    4. 2.4 Caterpillar
    5. 2.5 Color Shift in Low Gray Scale
    6. 2.6 Gray Scale Gradient Discontinuity Issue
    7. 2.7 First Scan Line Dim
  6. 3Summary
  7. 4References

Color Shift in Low Gray Scale

White balance has a big impact on the tone of the display so it is important to keep the same white balance in different brightness at the same configuration. Figure 2-13 shows the color shift which is easily captured in in ultra-low brightness. the difference in parasitic capacitance between lamps of different colors is the main reason. Generally the Blue LED has much more parasitic capacitance than the red LED.

GUID-20220628-SS0I-MXDN-XTZM-HSNJWF8JHG9B-low.gif Figure 2-13 Color Shift in Low Gray Scale