SLVUC06 October 2020
By default, the GUI will recognize two serial ports from the EVM adapter, but may not select the I2C bridge automatically. Once the EVM is powered and the USB cable is connected to the computer, click the connect icon at the bottom left of the GUI. If the bottom notification updates to Hardware Not Selected:
Figure 4-2 Opening Serial Port
Options
Figure 4-3 Selecting an Alternate
PortAfter clicking OK, the GUI should connect to the device properly. If communication to the EVM is lost, most issues can be resolved by pressing the nRST_MCU button (S3) on the EVM. Afterwards, further issues can be diagnosed by confirming that MCU_IN (J18) is still present, and that the I2C pull-up domain is still active.