SLVUC20A March 2021 – August 2022 LP876242-Q1
Texas Instruments provides a GUI tool to enable, configure, and evaluate the various features of the LP876242-Q1 with the EVM. Please refer to the GUI User's Guide SLVUBT8 for a more detailed description of this tool.
The GUI runs on most PC platforms and requires an available USB port. The EVM USB connector is type-C and a type-A to type-C cable is provided with the EVM to connect to the host computer. The EVM enumerates as two COM ports and one additional port for the device firmware updates. The GUI uses ACCtrl COM port which can be found from the device manager of the operating system. The COM port can be changed from the GUI from Options—Device Settings menu.
A tool for estimating the efficiency of LP876242-Q1 device is also available called PMIC Efficiency Estimator Tool. The tool can be accessed here.