SLVUC30 July 2021
Most connectors and test points are labeled with their functional names on the silk screen of the PCB and the actual component names are omitted to avoid clutter on the silk screen of the EVM. Likewise, jumpers are labeled to be self explanatory. Table 4-1and Table 4-2 contain a description of each test point and its purpose.
Note that by default the TPS1HC100EVM comes configured for standalone operation with no attached LaunchPad.
| Connector or Test Point | Description |
|---|---|
| J5, VBB test points | VBB Input (supply) |
| J6, J8, GND test points | Ground connection (system ground) |
| DIAG_EN | Enable and disable diagnostics on the TPS1HC100B-Q1 |
| EN | Enable line for the TPS1HC100B-Q1 |
| LATCH | Controls latch functionality for the TPS1HC100B-Q1 |
| SNS | Current sense test point for the current sense output of the TPS1HC100B-Q1 |
| FAULT | Open drain fault test point for the TPS1HC100B-Q1. Pull-up source can be configured using J13. |
| Jumper | Function/Setting |
|---|---|
| Current Limit Setting | POT will enabled the physical "Current Limit" potentiometer, DIGI POT will enable the digital potentiometer U3 (TPL0102-100), not populating the jumper will default to the solder down resistor pad R4. |
| SNS Pot Enable | Enables the physical "SNS" potentiometer connected to the current sense output of the TPS1HC100B-Q1. Not populating this jumper will default to the solder down resistor R12. |
| LDO_EN / LDO_DIS | Enables and disables the onboard 3.3-V LDO |
| J13 (Fault Pull-Up) | Configures where the fault pin is pulled up from. This jumper will either be from the 3.3-V LDO or the 3.3-V rail from the attached LaunchPad. |
| LDO to BP Power | Connects the output of the onboard 3.3-V LDO to the 3.3-V rail of the attached BoosterPack. This jumper is used to power the attached LaunchPad using the LDO of the TPS1HC100EVM |
| DIAG_EN | Connects the TPS1HC100B-Q1's DIAG_EN signal to either the LDO's 3.3-V signal or ground |
| EN | Connects the TPS1HC100B-Q1's EN signal to either the LDO's 3.3-V signal or ground |
| LATCH | Connects the TPS1HC100B-Q1's LATCH signal to either the LDO's 3.3-V signal or ground |
| GND Net Bypass | Bypasses the resistor and diode ground network and connects IC ground to system ground |