SLVUCN2A October 2023 – August 2024 DRV3901-Q1
The DRV3901-Q1 EVM provides a scripting window to automate multiple tests and log their results. The scripting window can be opened from the tools menu as shown in the Figure 5-5.
Various functions in the scripting window is mentioned in Figure 5-6
Section | Description |
|---|---|
A | Drop down to select saved scripts |
B | Record button to record commands directly from the GUI. Once this is clicked return to the GUI and do the functionalities which will auto-generate the script and can be accessed from the scripting window. |
C | Script function. |