To set up the GUI the first time, follow these steps:
- Make sure that the previously-mentioned driver was
installed successfully to make sure that everything works properly.
- Plug the connected EVM and SCB unit to the PC and go to the GUI link provided earlier.
- Click the GUI Composer application window shown in
Figure 4-5 to launch the GUI from the web browser.
- For first-time GUI
Composer setup, follow the prompts to download the TI Cloud Agent
and browser extension shown in Figure 4-6. These prompts appear after you close the README.md dialog.
- Click the icon in the GUI Composer window shown in Figure 4-5 to download the GUI offline (optional).