SNAU266A July   2021  – August 2022

 

  1.   Abstract
  2. 1First-Time Setup
    1. 1.1 Evaluation Module Contents
    2. 1.2 Evaluation Setup Requirements
  3. 2EVM Connections
    1. 2.1 Connection Diagram
    2. 2.2 Power Supply
    3. 2.3 Reference Clock
    4. 2.4 Output Connections
    5. 2.5 Programming Interface
  4. 3Feature Evaluation
    1. 3.1 Buffer, Divider, and Multiplier Modes
    2. 3.2 SYSREF Generation
    3. 3.3 SYSREF Delay Generators
  5. 4Schematic
  6. 5PCB Layout and Layer Stack-Up
    1. 5.1 PCB Layer Stack-Up
    2. 5.2 PCB Layout
  7. 6Bill of Materials
  8.   A Troubleshooting
  9.   B USB2ANY Firmware Upgrade
  10.   C Revision History

USB2ANY Firmware Upgrade

When the onboard USB2ANY programmer is first connected, or if the firmware revision used for the onboard USB2ANY programmer does not match the version used by TICS Pro (2.7.0.0), TICS Pro will request a firmware update. Follow the pop-up instructions to complete the update.

  1. When the USB2ANY Firmware Requirement pop-up window appears, click OK to continue.
    GUID-D650642F-E42E-4893-81A5-A60E3961E7B2-low.png Figure B-1 Firmware Requirement
  2. The Figure B-2 pop-up window will load. Disconnect the USB cable from the EVM.
    GUID-7C1FC040-6920-4356-9C70-EE65148DDDE3-low.png Figure B-2 Firmware Loader
  3. While pressing the BSL button (shown below), connect the USB2ANY cable.
    GUID-B5BEDCBE-FCCF-4925-87CA-59C837C41B68-low.pngFigure B-3 BSL Button Location
  4. The firmware loader should recognize the USB2ANY as a target for programming, and an Figure B-4 button should appear.
    GUID-B38EE12E-697D-4E4B-BEFA-5F18F9D94078-low.png Figure B-4 Update Firmware
  5. Click Upgrade Firmware to start the firmware upgrade. Click Close after the upgrade is complete.
    GUID-569D2F72-F5EC-4458-BB43-B62CE2338B34-low.png Figure B-5 Firmware Update Complete
  6. Go to USB communicationsInterface in the TICS Pro software to check the USB connection. Make sure the USB Connected button is green.
    GUID-34970234-CD5B-43EC-8A7E-7803349F2683-low.png Figure B-6 USB Communications