SNAU305 February 2025 LMH1229 , LMH1239
The LMH1239 has two inputs, and each input has a signal detector. Based on Signal Detect status and input channel selected, the device automatically goes into power down. For example, if SDI_IN± is selected and there is no signal on SDI_IN1±, the CDR and output drivers go into power down. Note that the unselected input always goes into power down. The following macros checks the status of the signal detects on SDI_IN± or SDI_IN1±.
| COMMAND | REGISTER | VALUE | MASK | //COMMENTS |
|---|---|---|---|---|
| RAW | FF | 05 | 07 | //Select EQ/Drivers Register Page |
| RAR | 08 |
04 |
04 |
//Read Signal Detect status of SDI_IN±. A value of 1’b indicates signal present. |
| COMMAND | REGISTER | VALUE | MASK | //COMMENTS |
|---|---|---|---|---|
| RAW | FF | 05 | 07 | //Select EQ/Drivers Register Page |
| RAR | 08 | 01 | 01 | //Read Signal Detect status of SDI_IN1±. A value of 1’b indicates signal present. |