SNLU131A February 2013 – June 2024
If the following window opens after starting the ALP software, double check the hardware setup and that the board USB port is connected to the host PC.
Figure 4-7 No
Devices error messageThe USB driver is not installed. Check the device manager. There is a device named NSC ALP Nano Atmel device under the Universal Serial Bus Controllers as shown below.
Figure 4-8 Analog
LaunchPAD in Demo ModeDisable the demo mode by selecting the Preferences pull down menu and un-checking Enable Demo Mode.
Figure 4-9 Analog
LaunchPAD Preferences MenuAfter demo mode is disabled, the ALP software polls the ALP hardware. The ALP software updates and displays only DS90UH928Q under the Devices drop-down menu.