SNVU769A September   2021  – October 2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Top View with Basic External Connections
  4. 2Input, Output Voltages, and Load Current Requirements
  5. 3Jumpers and connectors
    1. 3.1 Test Points
  6. 4Getting Started
    1. 4.1 GUI
    2. 4.2 GUI Installation and working with GUI
  7. 5Watchdog
  8. 6Schematics, Layout and BOM
    1. 6.1 Schematic Diagram
    2. 6.2 PCB Layer Diagram
    3. 6.3 Components List
  9. 7Revision History

GUI

Texas Instruments provides a simple to use LP87745-Q1 GUI tool to enable, configure, and evaluate the various features of the LP87745-Q1 device on the EVM. Please refer to the GUI README.md file in the GUI tool's Help->View README.md tab for a more detailed description of this tool.

The GUI will run on most PC platforms and requires a USB port for connecting the EVM to the host computer. The EVM USB connector is type-C and a type-A to type-C cable is provided along with the EVM to connect to the host computer. EVM will get automatically connected to the GUI after the USB cable is connected and manual assignment of COM port is not necessary. If Hardware not Connected displays on the bottom left of the GUI, clicking Click to connect to hardware icon next to it will re-establish the connection. The GUI uses the ACCtrl COM port which can be found from the device manager of the operating system.