SPRACP6 December 2019 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Instead of dedicating a set of GPIOs to determine boot mode, the boot mode of the device can be configured as a zero pin option.
With the introduction of the F28004x and newer devices, the number of boot mode select pins can now be customized to support as many as three and as few as zero pins. Using the zero pin option restricts the device to a single boot mode but it frees up the factory default pins to be used for GPIO purposes. Contrary to previous devices which only allowed reconfiguration of the fourth boot mode entry, for the F28004x device, the whole boot mode selection table is customizable. The steps below outline how the device can be configured for zero pin boot to flash:
This is achieved by configuring BOOT_DEF_LOW (0xFFFFFF03) and BOOT_DEF_HIGH (0xFFFFFFFF) user OTP locations as shown in Table 2.
| Boot Mode Number | BOOTDEF Name | Value |
|---|---|---|
| 0 | BOOT_DEF0 | 03(Flash boot) |
| 1 | BOOT_DEF1 | 0xFF |
| 2 | BOOT_DEF2 | 0xFF |
| 3 | BOOT_DEF3 | 0xFF |
| 4 | BOOT_DEF4 | 0xFF |
| 5 | BOOT_DEF5 | 0xFF |
| 6 | BOOT_DEF6 | 0xFF |
| 7 | BOOT_DEF7 | 0xFF |
All the above custom boot configurations take effect by programming the related locations in user-configurable DCSM OTP. The steps below outline one way that can be achieved:
#pragma RETAIN(otp_z1_data_1)
#pragma DATA_SECTION(otp_z1_data_1,"dcsm_zsel_z1_1");
const long otp_z1_data_1 = 0x5AFFFFFF;
#pragma RETAIN(otp_z1_data_2)
#pragma DATA_SECTION(otp_z1_data_2,"dcsm_zsel_z1_2");
const long otp_z1_data_2 = 0xFFFFFF03;
MEMORY
{
PAGE 0:
DCSM_ZSEL_Z1_P0: origin = 0x07800C, length = 0x000002
DCSM_ZSEL_Z1_P1: origin = 0x07801C, length = 0x000002
}
SECTIONS
{
dcsm_zsel_z1_1 : > DCSM_ZSEL_Z1_P0, PAGE = 0
dcsm_zsel_z1_2 : > DCSM_ZSEL_Z1_P1, PAGE = 0
}
For detailed information on the above configurations, see the Device Boot Modes chapter in the TMS320F28004x Piccolo Microcontrollers Technical Reference Manual.
NOTE
OTP locations cannot be re-written, so it is strongly suggested that the Emulation Boot Mode be used to validate the custom modification first. EMU-BOOTPIN-CONFIG and EMU-BOOTDEF can be programmed to experiment with different boot modes without writing to OTP.