SPRAD68 February 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
The Device Resources section contains all of the required device resources for the UMCL. Additionally, the panel on the left hand side can also show the resources used. Upon clicking any of the device resources, the configured parameters are shown. More device resources can be added by simply clicking the '+' icon next to the resource desired. This allows for an easy integration of further capabilities.