SPRADN5 December 2024 F29H850TU , F29H859TU-Q1
The DLT tool has two communication peripheral designs to export DLT logs out of the device. This application note focuses on a UART-based design to export the DLT FIFO out of a device and visualizes the data on a COM port or through a GUI interface like GUI composer. The other communication peripheral is FSI that can be used with the tool. This requires a FSI to UART-USB bridge device. This application note uses an example found within the F29x MCU SDK under the following folder: C:\ti\c2000\mcu_sdk_f29h85x_x_xx_xx_xx_xxx\examples\driverlib\single_core\transfer\transfer_adc_tempsensor_dlt . The following are detailed steps on how to add the DLT tool to any project.
Figure 6-1 DLT