SPRUI03E June 2015 – January 2023
Here is another use of the START and SIZE operators in the context of a GROUP specification:
GROUP
{
outsect1: { ... }
outsect2: { ... }
} load = ROM, run = RAM, START(group_start), SIZE(group_size);This can be useful if the whole GROUP is to be loaded in one location and run in another. The copying code can use group_start and group_size as parameters for where to copy from and how much is to be copied. This makes the use of .label in the source code unnecessary.