SWRA737A February 2022 – August 2022 CC1352P , CC1352R , CC2640R2F , CC2640R2L , CC2642R , CC2652P , CC2652R , CC2652R7 , CC2652RSIP
To run the PER test on different PHY’s, the sequence of commands are different from the above section in the following ways:
In step 1 of Section 3.5 on Rx side, send the device a HCI_LE_EnhancedReceiverTest command instead of the HCI_LE_ReceiverTest command.
Figure 3-11 Set
HCI_LE_EnhancedReceiverTestIn step 3 of Section 3.5 on Rx side, send the device a HCI_LE_EnhancedTransmitterTest command instead of the HCI_LE_TransmitterTest command.
Figure 3-12 Set
HCI_LE_EnhancedTransmitterTest
Figure 3-13 Response After Setting
HCI_LE_EnhancedTransmitterTestBelow lists the test logs for different PHY rate.