SWRU628 January 2025
This EVM contains components that can potentially be damaged by electrostatic discharge. Always transport and store the EVM in the supplied ESD bag when not in use. Handle using an antistatic wristband and operate on an antistatic work surface. For more information on proper handling, refer to SSYA010A.
The immersion silver finish of the PCB provides better high-frequency performance compared to ENIG, but is also prone to oxidation in an open environment. This oxidation causes the surface around the antenna region to blacken. However, mmWave Radar performance remains intact. To avoid oxidation, the PCB needs to be stored in an ESD cover and kept at a controlled room temperature with low humidity conditions. All ESD precautions must be taken while using and handling the EVM.