TIDT202 September 2020
Thermal images are shown in the following figures. The ambient temperature is 25°C, and the thermal images were taken with all outputs at a full load of 3 A. The controller was operated for approximately 2 hours before thermal images were taken to ensure thermal steady state was reached.
Figure 2-3 Top side
Figure 2-4 Bottom side