TIDT353 September 2023
Soft start behavior is shown in the following figures.
In the following waveforms, channel 1 in dark blue is load current; channel 3 in purple is output voltage; channel 4 in green is primary current.