DLPU049C July   2017  – October 2017

 

  1.   TI DLP LightCrafter™ Display 2000 EVM User's Guide
    1.     Trademarks
  2.   3
    1. 1 DLP LightCrafter Display 2000 EVM Overview
    2. 2 Quick-Start Guide
      1. 2.1 Use With Host Processor
      2. 2.2 Use Without Host Processor
    3. 3 What is in the DLP LightCrafter Display 2000 EVM?
      1. 3.1 Optical Light Engine Overview
      2. 3.2 External Interface Overview
    4. 4 Example Application
    5. 5 Troubleshooting
    6. 6 Additional Documentation
  3.   Revision History

Troubleshooting

If you encounter any issues when using the DLP LightCrafter Display 2000 EVM, the following tips below may assist you in resolving common or known problems:

  • When reading the "System Temperature" register using compound command 0xC5, the system may return an incorrect value on the initial read. If this occurs, send a second read command to the DLPC2607 to receive the correct temperature value in return.
  • When attempting to send an invalid command to the DLPC2607, the command error flag may read as 0 even though an error flag should have been raised. This is a known issue.
  • If the DLP LightCrafter Display 2000 EVM is connected to the BeagleBone Black, ensure that both devices are powered up for proper operation. If the BeagleBone Black is not receiving power, the DLP LightCrafter Display 2000 EVM may fail to boot even though it is receiving power.