SBAA708 July 2025 LM251772 , LM51772 , LM51772-Q1
Some applications require a disconnect switch on the input or output side of the switch mode power supply. This can be required for a system specification, like USB, which only allows a max of 10uF on the VBUS until the negotiation has finished and the power supply is enable or a reverse battery protection. The LM51772, LM251772, and the corresponding automotive (-Q1) devices features a high voltage drive pin (DRV1) to support an input or output disconnect FET (see Figure 2). This pin can be also used as a driver for a charge pump output to do a reverse polarity protection using an external n-channel FET. The supply for this pin can be selected by R2D and I2C configurations. In this application brief, various scenarios are shown how this can be used in an applications.
The following configurations are possible with to support with the DRV1 pin:
The disconnect switch can be place on the input or output side of the power stage, see Figure 2.
Forward: polarity protection on input side
Use case: provides a reverse polarity protection, often required for battery power systems. For example, automotive. When powering up with the correct polarity, the initial current flows through the body diode.
Reverse: output disconnect – reverse direction on output side.
Use case: This is required. For example, for USB-PD to disconnected the large output capacitors from the power stage from the VBUS of the USB port.
| DRV1 Configuration | |
|---|---|
| DRV1 Sequence | Pull-low or CP running if converter operation is on |
| DRV1 Config | VCC2 (charge pump driver) |
The charge pump used to provide the gate signal for the n-channel MSOFET need some time to ramp up. There is a slight delay after enabling the charge pump till the MOSFETs starts conducting (typically 2-3 charge pump switching cycles).
R1 in Figure 3 is to discharge the storage cap once charge pump stops. This discharge time depends on R1 and C1 but also on the ramp down of the MOSFET see simulation below.
Forward: used as reverse polarity protection on input side
Use case: input disconnect – reverse polarity protection provides a reverse polarity protection, often required for battery power systems. For example, automotive. When powering up with right polarity, the initial current flows through the body diode.
Reverse: used as an additional disconnect switch
Use case: output disconnect – avoid current from the output is driven into the power stage.
| DRV1 Configuration | |
|---|---|
| DRV1 Sequence | Pull-low or CP running if converter operation is on |
| DRV1 Config | Open drain (active = pull low) |
The PMOS when operated in short circuit condition transitions from the conduction mode to the linear mode and work a current limiting resistor. This can cause very high losses. Consider this for the MOSFET selection. This even appears with the average current limit enabled as the current is also limited by this MOSFET as soon as the output voltage drops down so that the gate signal is below the Miller plateau.
Additional options for using the DRV1 pin:
| DRV1 Configuration | |
|---|---|
| DRV1 Sequence | Depends on application requirements |
| DRV1 Config | Depends on application requirements |