SBAA885 October   2026 BQ76907-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Passive Balancing Mechanism of BQ76907
    1. 2.1 Balancing Current Path
    2. 2.2 Balancing Current
    3. 2.3 Balancing Time Estimation
  6. 3Particularity of Supercapacitor Systems
    1. 3.1 ESR and Voltage Recovery Effect
    2. 3.2 Impact on Balancing Strategy
  7. 4Balancing Scheme Design
  8. 5Reference Algorithm Implementation and Example
    1. 5.1 Algorithm Flow and Pseudocode
    2. 5.2 Design Example
  9. 6Conclusion
  10. 7References

ESR and Voltage Recovery Effect

The terminal voltage of the supercapacitor can be expressed as:

Equation 10. V C E L L = V O C + I ∙ E S R

Wherein:

  • VOC is the open-circuit voltage
  • I is the current flowing through the cell
  • ESR is the equivalent series resistance

When the system is in a charging or discharging state, the measured cell voltage does not completely represent its true energy storage state. If instantaneous voltage is directly used for balancing judgment, it may lead to incorrect balancing decisions. After the charge/discharge current is removed, the internal charge of the supercapacitor is redistributed, and the terminal voltage will slowly recover to a new stable value. This process is usually called the voltage relaxation effect (Voltage Relaxation). Therefore, making balancing judgments immediately after high-current working conditions end may overestimate or underestimate the actual voltage difference.