SBAS996B May 2020 – April 2021 AMC3306M25
PRODUCTION DATA
The differential amplifier input stage of the AMC3306M25 feeds a second-order, switched-capacitor, feed-forward ΔΣ modulator. The gain of the differential amplifier is set by internal precision resistors with a differential input impedance of RIND. The modulator converts the analog input signal into a bitstream that is transferred across the isolation barrier, as described in the Section 7.3.3 section.
| sinc3 filter, OSR = 2, fCLKIN = 20 MHz, fIN = 1 kHz |
There are two restrictions on the analog input signals INP and INN. First, if the input voltages VINP or VINN exceed the range specified in the Section 6.1 table, the input currents must be limited to the absolute maximum value because the electrostatic discharge (ESD) protection turns on. In addition, the linearity and parametric performance of the device are ensured only when the analog input voltage remains within the linear full-scale range (VFSR) and within the common-mode input voltage range (VCM) as specified in the Section 6.3 table.